Issue:
Connect the Remote Keypad (VW3A1111) to the Altivar Process drive
Product line:
ATV600, ATV900, Altivar Process
Environment:
All Altivar 600 and 900 process drives
Cause:
N/A
Resolution:
The VW3A1111 keypad has a cable port built into the bottom. Move the rubber cover to access the port. See the photo attached.
This is generally a temporary connection. To permanently remote mount the keypad, use VW3A1112.
Connect the Remote Keypad (VW3A1111) to the Altivar Process drive
Product line:
ATV600, ATV900, Altivar Process
Environment:
All Altivar 600 and 900 process drives
Cause:
N/A
Resolution:
The VW3A1111 keypad has a cable port built into the bottom. Move the rubber cover to access the port. See the photo attached.
This is generally a temporary connection. To permanently remote mount the keypad, use VW3A1112.
Released for:Schneider Electric Saudi Arabia