Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the last version of Vijeo Designer that supports the XBTG series?
Issue:
The XBTG series is missing in my Vijeo Designer V6.2? When was the series removed from the software?

Product Line:
Vijeo Designer 5.1 or higher

Resolution:
The last version of Vijeo Designer that supports the XBTG seres is Vijeo Designer V5.0 (including all Service Packs). Anything newer will no longer support these Magelis HMI. Provided that the XBTG series became obsolete in 2010, it is suggested to migrate to a newer series of HMI, such as the HMIGTO or HMIGTU for forward compatibility.