Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we need to install Vijeo Designer Runtime to download to a Magelis HMI?
Issue:
It is unclear what the Vijeo Designer Runtime for Windows package is intended for.

Product Range:
Vijeo Designer 5.1 or higher

Resolution:
The Vijeo Designer Runtime for Windows executable does not need to be installed to download to a Magelis HMI. This installer is only intended to be used on iPCs or PCs that will be used as an HMI. You do not need to install this package on the Vijeo Designer development PC.