Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the HMIGTU be used without a display?
Issue:
Trying to find a way to use the HMIGTU series without purchasing a HMIDT screen.

Product Line:
HMIGTU, HMIG3U, HMIG5U

Resolution:
Unfortunately, there is no way to use the HMIGTU series without an HMIDT screen. The HMIGTU series receives its power via the HMIDT display. The two modules must be used together. If you require to use a HMI without a screen, consider the Magelis Modular IPC range (HMIBM series).