Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the DC bus level at which the Brake resistor engages for the ATV312 Drives?
Issue:
DC bus level at which the Brake resistor engages for the ATV312 drives

Product line:
ATV312, Altivar 312

Environment:
all

Cause:
n/a

Resolution:
The internal transistor will output to a Brake resistor at the following voltage levels:

For 200-240V drives, the DC bus level is 379V
For 380-480V drives, the DC bus level is 792V
For 575V drives, the DC bus level is 948V

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre