Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Firmware version of M580 CPU & BMECRA/BMXCRA must I use to diagnose the power supply BMXCPS4002's redundancy
M580 CPU : 2.13 or above

CRA : 2.16 or above

if older versions are used and the diagnostics EF is used for the CPS4002 (i.e. PWS_DIAG or PWS_CMD), then it may crash