Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find specifications on the enclosed ATS22?
Issue:
Specifications on the enclosed ATS22.

Product Line:
ATS22 Enclosed

Environment:
All serial numbers, enclosed ATS22

Cause:
Clarification of the specification of the ATS22

Resolution:
The specifications can be found in the Enclosed ATS22 Manual, document number 30072-453-26. The manual is attached below.

Schneider Electric Saudi Arabia

Attachment(s)
ATS22 specification.pdf [644.68 KB]