Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I get the ATV312 Drive to start when power is applied?

Article available in these languages: Dutch

Issue:
ATV312 to start the motor as soon as power is turned on to the drive

Product Line:
ATV312, ATV31

Environment:
All Part numbers, all models

Resolution:
First go to the I-O menu and make sure tCC is set to 2C and that tCt is set to LEL.
Then power down the drive and install a jumper between terminals +24 and LI1.
When power is applied the drive will recognize the Run command is present and will run at the commanded frequency reference.

If the drive will always run at the same speed, you can set the LSP parameter to the required frequency and not provide an analog input or other speed reference.