{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Vijeo Designer v6.2 supports Windows 10?
Issue:
Is Vijeo Designer version 6.2 Windows 10 compatible?

Product Line:
HMI, Magelis, Vijeo Designer

Environment:
Windows 10

Cause:

Resolution:
Starting from Vijeo Designer 6.2 SP6, Windows 10 will be supported officially. All the documentation has been updated to reflect this in the Help menus and manuals.

Schneider Electric Saudi Arabia