Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the process to upgrade the firmware for an EM3555/3555A meter?

Issue
A customer would like to know the procedure to upgrade the firmware for an EM3555/EM3555A meter.

Product Line
EM3500 series

Environment
EM3555 / EM3555A

Cause
The firmware for the meter is outdated and needs to be upgraded.

Resolution

*WARNING*
Before attempting this procedure, the user must ensure that the meter is on RS (reset code) 2.004.  This can be checked from the sticker on the front panel of the meter which will read "FW: RS 2.004".  If the meter is not on this RS revision the meter CANNOT be upgraded in field.

The meter can be upgraded using the DLF-3000 utility. You can find the latest version of the DLF-3000 utility here: DLF-3000 Download and Instructions. Further documentation on the EM3555 can be found here: PowerLogic EM3500

If additional details are needed Veris technical support can assist further.


customersupport@veris.com