Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to fit reloading time by configuration / PLC Program of BMX EAE0300 ?
Question:
In the User Manual of Module BMX EAE0300,  you can find the following info:
Reloading Time  10 to 40 μs depending on encoder
Is it possible to fit reloading time by configuration / PLC Program?


Answer:
Actually, this is not the adjustable parameter for EAE module.
It is the requirement for the encoder spec to accommodate its communicate with the  EAE module.