Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot change from Local to Remote on my ATV312 drive, by holding the Mode button.

Article available in these languages: Korean

Issue:
ATV312 not changing from local to remote mode.

Product Line:
ATV312 series drives

Environment
Firmware version 5.1 IE56 and above.

Cause:
Recent firmware change.

Resolution:
As of firmware version 5.1 IE56, The ATV312 series drives can no longer be switched from local mode to remote.  In order to change the drive from local to remote, you perform a factory reset using the FCS parameter.