Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is HMIGXO3501 compatibile with vijeo designer V6.2, and if so, how to upgrade from an existing vijeo designer 6.0 to 6.2
HMIGXO is compatible with VJD 6.2. First of all your vijeo designer license should be registered. Here is below  the upgrade code to activate HMIGXO targets in Vijeo Designer:

VJDHTGTGX

To enter this upgrade code, you have to open Vijeo Designer and go to Help >> About... >> License >> Upgrade...

After that, you will be able to open/import a Vijeo Designer application developed for a HMIGXO target.