Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the programming software and cable for TSX3721001 ?
Software
The software is "PL7 Micro". Part number is TLXCDPL7MP45. This software will run on a Windows 7 32 bit machine. It will not run on a 64 bit operating system.

Cable
We have two alternatives:
1-For USB
Part number for the USB cable is TSXCUSB485 + TSXCRJMD25 , for further information, kindly check the data sheet links below:

TSXCUSB485, connection cord set for PC terminal - for Atrium / Premium - 0.4 m
http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?cat_id=BU_AUT_1438_L3&el_typ=product&nod_id=0000000018&prd_id=TSXCUSB485

TSXCRJMD25, connection cord set for PC terminal - for Premium / Quantum - 2.5 m
http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?cat_id=BU_AUT_533_L3&el_typ=product&nod_id=0000000020&prd_id=TSXCRJMD25

2-Multi-Function Serial Communications Cable:
The cable part number is TSXPCX1031 , for further information kindly check the data sheet link below:
http://eshop.schneider-electric.com/product.aspx?org=21&lang=0&dist=276&prod_id=TSXPCX1031