Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to delete a DTM in a Unity pro application when not installed - Quantum platform

Issue

Error message displayed when trying to delete a DTM
Potential issue due to the DTM version Compatibility"
"Warning: Potential issue due to the DTM version incompatibility.  <example> DTM.
An error occurs during the check of DTM compatibility. DTM version in application is V<example>).
DTM on the PC: not installed or installed without version information

Product Line

Quantum, 140NOC78x00

Resolution

As of today, when a DTM is not installed,  it is impossible to create the dynamic menu of the Dtm and then delete it.

We suggest to

  • Install the required DTM
  • Update the DTM catalog
  • Open the application and the TOOL>DTM browser
  • Delete the desired DTM from the DTM browser tree.