Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum input voltage range of the ATV6XX "N4" Process family drive?
Issue:
Maximum input voltage range of the ATV6XX "N4".

Product Line:
Altivar 6XX process drive family

Environment:
All models, All serial numbers.

Cause:
N/A

Resolution:
The range of the input voltage for the ATV6XX Process drive family is 380 - 15% to 480 +10% or a range of 323 to 528VAC, three phase.