Search FAQs
Osisense XC - Datasheet of the adapted limit switch XCMN2115T1L0
Please find attached the datasheet of the adapted limit switch XCMN2115T1L0, using a special cable halogen free for railway equipments, complying to EN 50306 and EN 45545 standards. Cable lenght = 1m. This reference is available to order without any restriction. It is not in stock, it is produced at order reception by the assembly plant. A second similar reference exists with 50cm cable lenght only : XCMN2115T05L0.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Explore more