Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I view Machine Expert HVAC - SoMachine HVAC variables in Vijeo Designer?

Issue:

How do I view Machine Expert HVAC - SoMachine HVAC variables in  Vijeo Designer?

Product Line:

Machine Expert HVAC, SoMachine HVAC, Vijeo Designer

Resolution:

Vijeo Designer uses ModbusRTU or Modbus/TCP to read and write data to a M171/172 HVAC controller. Only Machine Expert HVAC - SoMachine HVAC Status Variables have an assigned modbus address. Therefore only Status Variables can be Viewed and written to by a Magelis HMI. You can define Status Variables in you SoMachine HVAC project in the Resources Tab. When you create a Status Variable, Machine Expert HVAC - SoMachine HVAC automatically assigns an address to the variable. Such as 8960. In Vijeo Designer you would reference that address by using 48960 in your variable definition window.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)