Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change Units in the ATV Process Drive?

Article available in these languages: Spanish

Issue:
Adjust the units in the ATV Process drive.

Product Line:
Altivar Process
ATV6xx
ATV9xx

Environment:
All part numbers

Cause:
Default units  (Pressure in Bar, Flow in M3/h. Temp in deg C, Currency in Euro) may not be applicable to all customers in all regions of the world.

Resolution:
Using the HMI:
Under Menu 5 :[Complete settings], and subMenu 5.3 [Define system units] these settings can be manually changed.
To change using SoMove - See attached PDF.

Schneider Electric Saudi Arabia

Attachment(s)
How to Change units in SoMove.pdf [50.35 KB]