Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the impedance of the analog input AI1 on the ATV12 drive?

Article available in these languages: Spanish

Issue:
Impedance of the ATV12 Analog input AI1.

Product Line:
All ATV12 drives

Environment:
Analog input 1

Cause:
None

Resolution:
Analog input AI1 can be configured as a voltage input or current [AIIt = 5U, 10U or 0A].
Analog voltage input can be configured 0 to +5 V or 0 to +10 V (maximum voltage 30 V).  the impedance: 30 kΩ.
Analog current input x to y mA, has an impedance of 250 Ω.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre