BMEAHI/AHO or SWT module need to use both Bus-Ethernet and Bus-X, so it is not supported to use with Bus-X CRA: BMXCRA. (BMECRA is needed)
The error message in unity pro appears as "Impossible to configure IO module due to compatibility checks --> BMEAHI0812 <=> BMXCRA31210 (SV>=2.10)"
It means the CRA module you configured on the rack "BMXCRA31210 (SV>=2.10)" is not compatible with "BMEAHI0812".
The error message in unity pro appears as "Impossible to configure IO module due to compatibility checks --> BMEAHI0812 <=> BMXCRA31210 (SV>=2.10)"
It means the CRA module you configured on the rack "BMXCRA31210 (SV>=2.10)" is not compatible with "BMEAHI0812".
Released for:Schneider Electric Saudi Arabia