Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to assign a logic input to external fault on the ATS48?

Issue:
Assigning a logic input to external fault on the ATS48.

Product Line:
Altistart 48


Resolution:
To assign a logic input to external fault do the following:
From RDY
Press down to IO Menu,   press enter
Press down to LIx (3 or 4), press enter
Press the down arrow to LIE (external fault), press enter
ESC back to RDY

When the logic input goes active to 24Vdc, the ATS48 will go to a faulted state and display EtF.  After the logic input goes inactive to 0Vdc, a fault reset is required.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)