Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the baud rate options on the ATS48 modbus port?
Issue:
Needs to know the baud rate for ATS48 modbus

Product Line:
ATS48

Environment:
All

Cause:
Need to use 115.2 baud

Resolution:
ATS48 modbus is only available at 19200 or 9600.
Please note that the remote HMI only works with the 19200 baud rate.