Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a variable be assigned to the ATV32 Somove timer function block?

Issue:
Assign a Timer Function Block on an ATV32

Product Line:
Altivar 32

Environment:
Somove function block for the ATV32 all serial number

Cause:
N/A

Resolution:
No, a variable cannot be assigned to the timer function of the ATV Logic, Timer function block properties.   The on and off delay time is hard set in the function block properties.