Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause the ATV212 drive inside of the S-flex not to power up when you switch the AFC/Off/Bypass switch to AFC mode?

Issue:
Why isn't the ATV212 drive in the S-Flex enclosure powering up when the selector switch is in the AFC position?

Product Line:
Altivar ATV212 S-flex enclosed with bypass option and B07 mod

Environment:
All

Cause:
Line contactor is not pulling in to power up the variable speed drive.

Resolution:

  1. Check to see if the red power LED is powered on the outside of the enclosure.  If this red power LED is on, then we know the CPT and fuses are all good.
  2. Check to see if the Line contactor is pulled in.  If the line contactor is not pulled in, check the control circuit to see what might be not allowing the contactor to pull in.
  3. Check to see if the bypass circuit works by putting the AFC/Off/Bypass switch in bypass mode.
  4. If the bypass contactor is not pulling in, and the line contactor is not pulling in, check to see if the OLR has tripped and needs to be reset.
  5. Check for loose connections in the 120VAC control wiring in the S-Flex enclosure.

Review the wiring diagrams in the S-Flex manual for details on how the drive cabinet is wired.
https://www.se.com/us/en/download/document/30072-451-83/ ​​​​​​​

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team. If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)