How can we help you today?

Does the ION8600 support SysLog ?

Isuue
The user would like to know if the ION8600 includes the Syslog feature

Product line
ION8600

Resolution
The ION8600 does not include the syslog support and there are no future plans to include such a feature. The ION8650 is direct replacement to the ION8600 and supports the syslog feature as of firmware V420. The attached official letter from the Global Utility Metering Offer Manager confirms that there will not be any new features added to the ION8600 including support for SysLog.

Schneider Electric Saudi Arabia

Attachment(s)
Syslog_support.pdf [33.26 KB]