Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What could cause Hex error 3410 (Network module missing) on an M580 L9_MSTR function block?
The high byte or MSB of the 4th implied word in the control array for the M580 L9_MSTR function block must be set to 65,024 Dec  or 16#FE00 Hex in order for the block to communicate out from the M580 native ethernet port.

If the project was converted from Concept Software, and you are using the MBP_MSTR,  make sure that you are using a located 9 WORD array for the Control pin.  Concept allowed a single WORD there and Control Expert does not.