Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Modbus Function Codes supported by the new UNITY Momentum controllers?

Issue:

What are the Modbus Function Codes supported by the new UNITY Momentum controllers?

Product Line:

Unity, Momentum, Quantum, M580, M340

Resolution:

Modbus function codes supported by the Unity Momentum Controller:

  • 01 = Read multiple bits (%Q)
  • 02 = Read multiple discrete bits (%I)
  • 03 = Read multiple words (%MW)
  • 04 = Read multiple input words (%IW)
  • 05 = Write single bit (%Q)
  • 06 = Write single words (%MW)
  • 07 = Read Exception Status (For serial line only)
  • 08 = Diagnostic with the following sub-functions attached for serial line only:
    • Sub-function code 00 “echo mode" (Return Query Data)
    • Sub-function code 01 (Restart Communication Option)
    • Sub-function code 02 (Return Diagnostic Register)
    • Sub-function code 03 (Change ASCII Input Delimiter)
    • Sub-function code 04 (Force Listen Only Mode)
    • Sub-function code 10 (Clear Counters and Diagnostic Register)
    • Sub-function code 11 "counter 1" (Return Bus Message Count)
    • Sub-function code 12 "counter 2" (Return Bus Communication Error Count)
    • Sub-function code 13 "counter 3" (Return Bus Exception Error Count)
    • Sub-function code 16 "counter 6" (Return Slave NAK Count)
    • Sub-function code 17 "counter 7" (Return Slave Busy Count)
    • Sub-function code 18 "counter 8" (Return Bus Character Overrun Count)
  • 11 = Get Com Event Counter (For serial line only)
  • 12 = Get Com Event Log (For serial line only
  • 15 = Write multiple bits (%Q)
  • 16 = Write multiple words (%MW)
  • 22 = Mask write register (As a Server only)
  • 23 = Read/Write multiple registers (%MW)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)