Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why am I missing data missing after retrieving it using the Vijeo Designer data manager?
1) Make sure to Flush the data. This moves the data from the SRAM to file. The File is either the secondary or optional drive depending on what is selected in the data location.  To do that you can execute the FlushAllDataLogging() script command.

2) Periodic data logging in Vijeo Designer only adds a new record when the value change.