Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the trip state (fault status) at terminals 15 and 16 on an SFLEX drive fault?
Issue:
What is the trip state at pins 15 and 16 on an SFLEX drive fault?

Product Line:
Altivar Machines, S-Flex

Environment:
All models and serial number

Cause:
FLC / FLB never closes when the drive is running.

Resolution:
FLC – FLB is an normally closed contact. When programmed for Trip in the ATV212 this contact opens on power-up, if no fault present and close when a fault is present or when power is removed from the drive.
ATV212 contact image
See the S-Flex Manual for details and other possible wing diagrams https://www.se.com/us/en/download/document/30072-451-83/