Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What causes Err9 fault on the ATV212 Drive?

Issue:
Err9 fault on ATV212

Product Line:
Altivar 212

Environment:
All

Cause:
Fault code

Resolution:
This fault will appear if the remote graphic keypad is used for control and the cable gets disconnected.  This is if CMOd = 1 or FMOd = 3.
Check that the cable is still connected and not loose.
Check the keypad for issues or try another keypad.
Check for electrical noise.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: