Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What level of current flow triggers an SCF2 fault on an ATV61 or ATV71 series drive?
Issue:
What level of current flow triggers an SCF2 fault on an ATV61/ATV71?

Product Line:
ATV61 / ATV71 series

Environment:
All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:

SCF2

Principal :
The drive is protected against impedance (slow) short circuit, phase to phase or phase to ground on the output of the drive.
When there is a impedant short circuit the drive trips in SCF2 and the fault relay opens

Detection time:
It’s a software detection (a few ms).  Output current sum > 25% of the rated current of the drive.