How can we help you today?

How about install the single/multi mode of the fiber of NRP module

Quantum NRP module 140NRP, user can use two modes (single and multi ) of fiber in one system. but can't connect the single mode to multi mode directly.

the architecture as the attachment
Pink Line :- Single mode Fiber Optic
Blue Line :- Multi mode Fiber Optic
Green :-  ethernet Cable.

Schneider Electric Saudi Arabia

Attachment(s)
36-ILS-SCM-001 Model (1).pdf [600.29 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre