Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What to do when Vijeo Designer cannot delete objects from the Favorites folder in the toolchest?
Issue:
What to do when Vijeo Designer cannot delete objects from the Favorites folder in the toolchest?

Product Line:
Vijeo Designer 6.2

Resolution:
When you are unable to delete objects from the Favorites folder of the Toolchest, goto the following folder and set the read/write permissions on the file TCParts.tcp.

"C:\Users\Public\Documents\Vijeo-Designer 6.2\ToolChest"

Restart Vijeo Designer and try again.