How to diagnose the error when the CID file imported to IEDCT failures ?
User uses the 140NOP85000 module for IEC61850 communication, sometimes they need to import the CID file to the IEDCT and IEDCT will check the file with some rules.
If some error is reported, there will be a error log file saved by user and customer could open the errorlog file to investigate it or send it to L3 to analyse .
If some error is reported, there will be a error log file saved by user and customer could open the errorlog file to investigate it or send it to L3 to analyse .
Released for: Schneider Electric Saudi Arabia