Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the DIO scanner capability of BMENOC03*1?
Before Unity Pro v11.1 the DIO scanner capability of BMENOC03*1 is 2K input/output words, since Unity Pro v11.1 the DIO capability of BME NOC03*1 will be improved to 4K input/output words.