Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If an application built for a lower level M580 HSBY CPU can be downloaded & executed in a higher level M580 HSBY CPU?

Article available in these languages: Spanish

Yes,an application built for the BMEH582040 is downloadable and executable on the BMEH584040, BMEH586040.
An application built for the BMEH584040 is downloadable and executable on the BMEH586040.