{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Error 127 in ION7650 event log
Issue
There is error code 127 in ION7650/7550 event log.

Product Line
ION7650
ION7550

Environment
Event log

Resolution
Error 127 is logged when the ION meter needs to recreate file space for a data recorder.

The 127 error is logged when there is NO data file present. The ION meter creates the file space for a data recorder and puts a message in the event log telling the user the file was created.

This is an informational message stating the meter corrected a missing file. This message is usually observed after a framework paste has occurred.

Schneider Electric Saudi Arabia