Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity Pro V11.0 Incomplete Build change, Fail GCC Compilation error
Goals and Symptoms
On BME P58 5040(C) , BME P58 6040(C) and BME H58 6040(C) PLCs application, with Unity Pro V11.0, build change of an application can be incomplete, a section can be not taken in account.
This situation is reported by following WARNING message: Fail GCC Compilation error in the output windows.
But this message does not stop the Build of the application.

Causes and Fixes
install the hotfix UnityPro_V110 HF0337840R to fixes the issue on Unity Pro V11.0.
Unity Pro V11.1 corrects this misbehavior.