Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What file format is the SD card on the Com'X 510 / 210?
Environment:
Ethernet Gateways

Product Line:
Com'X 510/210

Resolution:
The file format loaded on the SD card from the factory is the EXT3 Linux based file format. If for any reason the SD needs to be reformatted, EXT3 is the file format that should be used.
the SD  specification  is  4GB SD HDI class 6(**) , EXT3 Linux based file format.
**SD cards are based on the same flash memory technology. However, only high performance
memory cards offer the requested level of reliability: A high performance Single-Level Cell memory
card has in general at least 100 000 Write and Erase Cycles (10 000 for a multi-level cell card).