Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to remotely reset the Tesys T ?
Tesys T fault reset can be done through the Blue push button on the Unit itself or through any of the below means:

1. Input I5 ( in any of the 10 standard operating mode/s)
2. Reset key on the LTMCU
3. Power recycle
4. Bit 704.3 over the network if the Remote channel is network control.

If you are looking for a door mounted system which can press the Blue button on the Tesys T itself. Unfortunately, there are no accessories to do this.

The best suggestion would be to use an NO push button and mount it one the panel door and wire it to between the Terminal C and I5 on the Tesys T. The fault will be reset on pressing this Push button.

If you are using the LTMCU, the Reset can be achieved by pressing the Reset key on this operator panel

Schneider Electric Saudi Arabia

Attachment(s)
Tesys T Remote reset mode.pdf [23.96 KB]