Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you get full motor torque at zero speed on the ATV320 drives?

Article available in these languages: Spanish

Issue:
ATV320 using full motor torque at zero speed.

Product Line:
Altivar 320

Environment:
All serial numbers for Altivar 320

Cause:
To run the drive in a closed loop mode

Resolution:
The Altivar 320 is very similar to Altivar 32 and the Altivar 312.
All of these products do not manage closed loop regulation.
For closed loop control, consider an Altivar 71 or Altivar 900 series drive plus an encoder option card.