Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I run a 460Vac motor on a 575Vac ATV61 or ATV71 drive?

Issue:
Running a 460Vac motor on a 575Vac ATV61/ATV71 drive.

Product Line:
ATV61 ATV71

Environment;
All

Cause:
Test motor 460Vac Line supply 575Vac

Resolution:
No, this is not recommended.
Drives are designed to run motors with the same voltage rating.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.