Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which standard requirements are met by Resi 9 electrical panel and the trunking?
Resi 9 answers to the following standard requirements :
Electrical Panels :  IEC 60670-1, -24 (GP, PD) or IEC 61439-1 and 3 depending on the offer
Electrical Panels : IEC 50102
Electrical Panels : IEC 60529
Electrical Panels : LCIE
Facing of Control Panel: ERDF-CPT-M&S-Spe-10015A
Facing of control block : ERDF-CPT-M&S-Spe-13006A
GTL system (Trunking + Panels) : NFC 15-100 chap 771-558
Trunking system :  NF EN 50085-2-1

Schneider Electric Saudi Arabia

Attachment(s)
677480_20151127152632.pdf [1.19 MB]
677479_20151126143815.pdf [1.1 MB]