Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the remote keypad to use with Altivar 212 drives?

Article available in these languages: SL

Issue:
Altivar 212 keypad part number for remote control

Product line:
Altivar 212

Environment:
All

Cause:
Adding remote keypad

Resolution:
The standard ATV212 drive does not include a remote mounting keypad.  The compatible remote keypad is part number VW3A1101.  This is an HMI, full text keypad that includes Run, Stop/Reset, Forward/Reverse and ESC buttons.  This is the keypad only and does not include any cables, remote mounting plates or adaptors which are required to make connection between the keypad and ATV212.
Refer to the information below:

Remote mounting plate (keypad holder) - VW3A1102

Cables - 1meter -    VW3A1104R10
3meter -   VW3A1104R30
5meter -   VW3A1104R50
10meter - VW3A1104R100

Optional door kit (hinges onto the keypad holder and covers the keypad when closed) - VW3A1103
Optional 90 degree adaptor (not required when using VW3A1102 kit) - VW3A1105

The ATV212 drive cannot save programs into the VW3A1101 keypad.  Use another device such as the Multiloader or SoMove software to save/copy programming into another ATV212 drive.

Note that the VW3A1101 keypad is included with the S-Flex enclosed drives that have Factory Modification D07.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

Schneider Electric Saudi Arabia

Attachment(s)
VW3A1101.jpg [65.02 KB]