Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Control a Vijeo Designer HMI panel navigation using a SoMachine PLC

Issue:
How to Control a Vijeo Designer HMI panel navigation using a SoMachine PLC

Product Line
Vijeo Designer, SoMachine, EcoStruxure Machine Expert

Resolution:
To control the panel displayed on a Vijeo Designer HMI from a SoMachine PLC,
1) Start by creating a SoMachine variable of type INT and share it with Vijeo Designer through the Symbol Configuration.
In our example, the INT variable is called "iPanelNumber" from the POU called "PanelControl":
Variable Sharing of INT in Symbol Configuration Node

2) Once this is done, you should link this shared variable to an internal variable in Vijeo Designer called _CurPanelID
- Select _CurPanelID from the Variables pane.
- Assign the Variable from SoMachine "_SoM.MyController.Application.PANELCONTROL.iPanelNumber" to the "Read From Variable" row of the Property Inspector
_CurPanelID Read Variable from PLC location in Vijeo Designer

This method is also viable in EcoStruxure Machine Expert.

Attached is a Sample Project created in SoMachine v4.3 Patch 2 with Vijeo Designer v6.2.6.1 update installed:
"ReadFromVariableToCurPanelIDExample.project"

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
ReadFromVariableToCurPanelIDExample.project [521.17 KB]