Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M580 - Why the EFB "Drop" doesn't work in M580 with Quantum EIO architecture?
Question:Why the EFB "Drop" doesn't work in M580 with Quantum EIO architecture? all the channels display "0", no any data can be read:


Answer: The version of M580 CPU need to equal or later than 2.10, then the function will be correct.