How can we help you today?

Which version of M580 CPU are supported with Quantum EIO?

Issue
It does not seem that all models of M580 support Quantum EIO or RIO.

Product line
Modicon M580, Modicon Quantum IO

Resolution
The BMEP584040, 5040 and 6040  with minimum firmware version 2.10 are the only models that support Quantum IO

Schneider Electric Saudi Arabia