Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find information to set up the Bacnet option card on the ATV61 drives?
Issue:
Where can I find information to set up the Bacnet option card (VW3A3319) on the ATV61 drives?

Product Line:
Altivar Machines, Altivar 61, Altivar 71

Environment:
All

Cause:
N/A

Resolution:
For Bacnet setup assistance see the attached Bacnet programming manual.

Schneider Electric Saudi Arabia

Attachment(s)
new card atv61_bacnet_en_NEWCARD.pdf [922.72 KB]