Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a 120V control option card available for the ATV630 Process drives?

Issue:
Is there a 120V control option card available for the ATV630?

Product Line:
ATV630, ATV Process

Resolution:
A 120VAC input adapter card is not available for the process drives.
Consider an interposing relay for each digital input used.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.